Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

r_lvd Module Guide Resources

Last Updated:02/27/2018

Question:

Where can I find the references to module guide resources for the low voltage HAL module on r_lvd?

Answer:

Information on the module guide itself and the associated resources and known issues are available here.

Introduction

The Low Voltage Detection (LVD) HAL module provides high-level APIs for voltage-detection applications and is implemented on r_lvd. The LVD HAL module uses the LVD peripheral on the Synergy MCU. A user-defined callback can be created to notify the CPU when a voltage-detection event is triggered. The VCC is the source for all voltage-detection functions.

The LVD HAL module supports the following features:

  • VCC as the voltage-detection input
  • One build-time configurable low-voltage detector (via OFS1 register)
  • Two run-time configurable low-voltage detectors
  • Two result flags; one for a threshold check and one for the current state
  • Support for both interrupt or polling-event checking

 

Module Guide

The LVD HAL module guide is targeted for SSP 1.2.0 and above and the SK-S7G2 Kit.

The most recent versions of the LVD HAL module guide application note, application project and import guide are available here.

Module Guide Resources

No additional resources available at this time.

Known issues

  • Refer to the SSP release notes for known issues, available here.
Suitable Products
SSP
  • Was this article helpful?