Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

r_sce_arc4 Module Guide Resources

Last Updated:11/24/2017

Question:

Where can I find the module guide resources for the ARC4 HAL module on r_sce_arc4?

Answer:

The ARC4 HAL module doesn't have its own module guide. It is included in the r_sce module guide. The resources article for the r_sce module is available here.
SSP
  • Was this article helpful?