Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

r_sdmmc Module Guide Resources

Last Updated:11/21/2017

Question:

Where can I find the module guide resources for the SDMMC HAL module on r_sdmmc?

Answer:

The SDMMC HAL module doesn't have its own module guide. It is included in the Express Logic FileX framework module guide. The resources article for the sf_el_fx module is available here.
SSP
  • Was this article helpful?