Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Renesas Synergy MCUs

Latest Updated:07/18/2016
Renesas Synergy MCUs
Renesas Synergy MCUs provide the bedrock on which the Synergy Platform is built

S1 SeriesUltra-low power MCUs enabling incredibly long battery life in portable applications or applications that must survive a long time in standby mode are possible from the S1 Series without sacrificing analog capabilities, secure connectivity, and robust safety.

S3 Series: Enhanced CPU processing power, secure connectivity, advanced analog and timing control, safety self-test features, segment LCD and capacitive touch control, all built on a very low power silicon process are prime ingredients for smart IoT sensors and localized control.

S5 Series: A secure connectivity suite, large memory and serial memory expansion, high-accuracy analog, TFTLCD graphics with 2D engine and many built-in safety functions make S5 MCUs ready for extremely capable embedded control applications across the board.

S7 Series: Blazing fast processor core plus secure connectivity and industry-leading large memory sizes opens up developers’ options on design of a many of connected IoT applications, breaking through limitations previously faced by developers and engineering teams.

 

Recent Updates- important news and updates about Synergy MCUs

  • Just search the Knowledge Base for Synergy MCU

 

To find Data Sheets and User's Manuals just select the MCU of interest from the Synergy MCU web page here:

https://www.renesas.com/products/synergy/microcontrollers.html