Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Where can I find BSDL files for Synergy MCUs?

Last Updated:05/09/2017

Question:

Where can I find BSDL files for Synergy MCUs?

Answer:

BSLD files for Synergy MCUs can be found on the Downloads Tab from the MCU web page. For example, the web page for the S7G2 is located here: 

https://www.renesas.com/produc...7-series.html

Note that you can select IBIS/BSLD to search for just those file types.

Suitable Products
Synergy MCU
  • Was this article helpful?