Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

TPS-1 Built-in Boot Loader

Last Updated:06/01/2017

Question:

Does the TPS-1 have the boot loader program built-in? Is it possible to delete this program?

Answer:

The TPS-1 has the boot loader program in the boot ROM therefore it cannot be deleted.
Suitable Products
TPS-1
  • Was this article helpful?