Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

TPS-1 Firmware Download via JTAG

Last Updated:06/01/2017

Question:

We would like to try downloading firmware onto the TPS-1 via the JTAG port. Does the existing TPS-1 firmware/hardware/software support this functionality?

Answer:

It is possible to download the the TPS Updater over the JTAG interface (production process).
Suitable Products
TPS-1
  • Was this article helpful?