Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

TPS-1 Support of Combined Fiber and Copper Ports

Last Updated:06/01/2017

Question:

Can TPS-1 support combined use of both a fiber port and a copper port?

Answer:

Yes, TPS-1 can support fiber and copper at same time.
Suitable Products
TPS-1
  • Was this article helpful?