Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

TPS-1 Watchdog Timer Value in Parallel IO Mode

Last Updated:06/01/2017

Question:

If TPS-1  is used in parallel IO mode, what value is required for the 'Watchdog Time' in the Configurator? Should a zero value mean it's disabled?

Answer:

The watchdog timer depends on your software design. You must ensure that you can trigger the signal reliably, as the watchdog interval can be selected to be anywhere between 1 ms and 512 ms. During development you can disable the CPU watchdog by setting the interval value to “0” in the TPS Configurator.
Suitable Products
TPS-1
  • Was this article helpful?