Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

How long are the on and off when using a transistor for amplification?

Latest Updated:11/01/2007

Question:

When using a transistor for amplification, about how long are the turn-on and turn-off times?

Answer:

An amplification transistor is not used for switching, so these times are not prescribed. If you need switching characteristics, please use a switching transistor.
Suitable Products