Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

How to determine the marking of B-class product?

Latest Updated:05/01/2008

Question:

"1" is marked on RD6.2S B1. What is the marking of the B-class product?

Answer:

The request for a B-class product is responded by standard B1, B2, or B3. Therefore, there is no such marking as "B", but only "1", "2", or "3" is marked.
Suitable Products
CMOS Operational Amplifiers
Bipolar Operational Amplifiers