Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Which power-supply ICs products have encoded marking product name?

Latest Updated:10/01/2006

Question:

Among power-supply ICs, which products have encoded marking product name?

Answer:

The following products, which use power minimold (SOT-89/SC-62) or 5-pin minimold (SC-74A) as packages, have an encoded marking product name. For the encoding details, refer to the data sheet of each product.

<SOT-89>

  • uPC1093T
  • uPC1943T
  • uPC1944T
  • uPC78LxxT Series
  • uPC29LxxT Series
  • uPD120NxxT1B Series


[SOT-89 Package Drawing]




<SC-74A>

  • uPC1093TA
  • uPC1945TA
  • uPD120NxxTA Series

[SC-74A Package Drawing]

[Marking Example: uPC1093]

Product Name Marking
uPC1093T 93
uPC1093TA K93
Suitable Products
Power Management Linear