Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Will product degraded if protection of 3 terminal regulator operates?

Latest Updated:02/01/2007

Question:

Isn't the product degraded if the overheat protection circuit of the 3-terminal regulator operates?

Answer:

The overheat protection circuit operates because the junction temperature (Tj) exceeds the absolute maximum rating. There is a high possibility that the product is degraded.
Suitable Products
CMOS Operational Amplifiers
Bipolar Operational Amplifiers
3 Terminal Regulators