Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Where is the case temperature of a MOSFET taken?

Latest Updated:09/02/2013

Question:

Where is the case temperature of a MOSFET taken?

Answer:

Generally, the case temperature of an through hole package is taken at the base of the drain lead pin. For a surface mount package, the case temperature is taken at the metal part of the heat sink (metal part on the reverse side).
Suitable Products
Power MOSFETs for General Switching