Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

How great can the output current flow of the uPC4558 be?

Latest Updated:10/01/2006

Question:

How great can the output current flow of the uPC4558 be?

Answer:

The output current of the uPC4558 is not specified. Instead, a graph showing the VO-RL characteristics is shown on the uPC4558 Data Sheet for your reference. Please calculate the current based on your load resistance (RL) and corresponding output voltage (VO) using this graph.
Suitable Products
Operational Amplifiers
USB2.0 Host/Peripheral Controller
UPD720150