Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Can you explain what pairing between each channel of dual amplifier ?

Latest Updated:03/01/2006

Question:

I'm thinking to use a dual operational amplifier. Can you explain what the pairing between each channel (described in the electrical specifications) is?

Answer:

As a rule, the pairing described in the electrical specifications of a dual operational amplifier is affected by input offset (V and I). Input offset occurs when there is variation in the elements in the input operation stage. The input offset voltage variation is described in the data sheet's electrical specifications.

Suitable Products
Operational Amplifiers
USB2.0 Host/Peripheral Controller
UPD720150