Skip to main content
Renesas India - Knowledgebase

Can I use high reference with an output negative voltage using uPC1060?

Latest Updated:12/01/2011


The uPC1060 is used for the positive voltage. Is there any high-accuracy reference voltage generator that can output a negative voltage?


Unfortunately, no.
There is a method to convert the voltage generated by the uPC1060 into a negative voltage by using an inverting amplifier with a gain of 1 (i.e., 0 dB).
Consider using this method.
Suitable Products
Power Management Linear