Skip to main content
Renesas India - Knowledgebase

Does a thermal grease needs to be applied in 2SJ547 or the 2SK3212?

Latest Updated:09/02/2013


I'm considering using the 2SJ547 or the 2SK3212. Does thermal grease need to be applied? Also, is there any reference material?


Grease needs to be applied in order to heighten the heat dissipation effect. For a general explanation, refer to 2.5 Mounting to the Heat Sink in the following document.

Suitable Products
Power MOSFETs for General Switching