Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Why do the output of the uPC1100 overshoots when the power is provided?

Latest Updated:12/01/2011

Question:

The output of the uPC1100 overshoots when the power is provided.

Answer:

Generally, it is recommended to use the soft start function (by connecting a capacitor to pin 6).
Suitable Products
Power Management Linear