Skip to main content
Renesas India - Knowledgebase

Will the output of uPC317 must be opened if the voltage exceeds?

Latest Updated:12/01/2011


With the variable output type uPC317, the output voltage exceeds the rated value if the output is opened.


The output of a variable output type must not be opened because the minimum output current is specified.
The uPC317 does not start at a load current of 3 mA or less at room temperature. When it does not start, the output voltage exceeds the rated value.
Suitable Products
CMOS Operational Amplifiers
Bipolar Operational Amplifiers
3 Terminal Regulators