Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Are there any recommended mount pads for surface mount transistors?

Latest Updated:04/01/2007

Question:

Are there any recommended mount pads for surface mount transistors?

Answer:

The pads differ depending on the package, so please go to the following Web site and click the mount pad for the relevant package.
http:///www.renesas.com/discrete/en/package/smd.html

For the RF & microwave devices, refer to PACKAGE LINE-UP FOR RF AND MICROWAVE DEVICES on the following page (also for CAD data).
/request?SCREEN_ID=ViewDocumentSearch&EXECUTE_ACTION=search&KEY_WORD=R50ZZ0001
Suitable Products
  • Was this article helpful?