Skip to main content
Renesas India - Knowledgebase

What is the provisions when using RJK0628JPE in 100 A current control?

Latest Updated:09/02/2013


I'm considering carrying out about 100 A current control using the RJK0628JPE. Is there any recommended pattern or any precautions I should know about the pattern wiring (foil thickness, pattern width, etc.) of a printed circuit board for large current?


Although we have prepared recommended mount pads for each package, we do not have recommended circuit patterns.
Suitable Products
Power MOSFETs for General Switching