Are there any limitations when using the sample & hold function?
Latest Updated:02/14/2006
Question:
Are there any limitations when using the sample & hold function?
Answer:
The sample & hold function cannot be used when the øAD is less than 1 MHz.
Suitable Products
R8C/18 |
R8C/19 |
R8C/1A |
R8C/1B |
R8C/20 |
R8C/21 |
R8C/22 |
R8C/23 |
R8C/24 |
R8C/25 |
R8C/26 |
R8C/27 |
R8C/28 |
R8C/29 |
R8C/2A |
R8C/2B |
R8C/2C |
R8C/2D |
R8C/2E |
R8C/2F |
R8C/2K |
R8C/2L |
M32C/8A |
M32C/88 |
M32C/87 |
M32C/85 |
M32C/84 |
M32C/83 |
M32C/80 |
M16C/62A |
M16C/62A(M16C/62T) |
M16C/62M |
M16C/62N |
M16C/62N(M3062GF8NFP, M3062GF8NGP) |
M16C/62P |
M16C/6N4, M16C/6N5 |
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN |
M16C/30P |
M16C/29 |
M16C/28 |
M16C/26A |
M16C/1N |