Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Ports P20-P23 & P44-P47 set input mode; key-on wakeup for input to P20

Latest Updated:03/01/2005

Question:

(Interrupts)   Can ports P20 to P23 and P44 to P47 be set to input mode and key-on wakeup enabled only for input to P20? [2005/03/01]

Answer:

Yes.
Key-on wakeup can be enabled/disabled for individual pins in the key-input control register settings. (#104955)
Suitable Products
38D5