Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

What does absolute accuracy of the D/A converter written as 1% means?

Latest Updated:03/13/2008

Question:

(D/A Converter)  In the datasheet, for VREF = 4.0 to 5.5V, the absolute accuracy of the D/A converter is written as 1%. What does this mean ? [2008/03/13]

Answer:

It means, when VREF = 5.12 V, the maximum output error is 5.12 V × 0.01 = 51.2 mV. Note that this is a specified value, that is, the maximum value under the conditions specified. (#106878)
Suitable Products
3803H
3803L