Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Is the flash programmer capable of writing binary files?

Last Updated:05/10/2017

Question:

Is the flash programmer capable of writing binary files?

Answer:

The Flash Programmer PG-FP5 and Renesas Flash Programmer are not capable of writing binary files.

The Flash Development Toolkit is capable of writing binary files.
However, this product is not equipped with an offset function, so data from address 0 is required.

Prepare program files supported by the desired flash programmer.

Suitable Products
Renesas Flash Programmer
PG-FP5