Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

How to change the font of the output window and workspace in HEW3?

Latest Updated:09/10/2007

Question:

[High-performance Embedded Workshop V.3]  I would like to change fonts of the output window and the workspace in High-performance Embedded Workshop3.

Answer:

Please set the font on the screen by selecting HEW->TOOLS->OPTIONS-> FORMAT. It is also possible to set by right clicking ->SET FONT on the OUTPUT screen about OUTPUT window.
Suitable Products
High-performance Embedded Workshop