Skip to main content
Renesas India - Knowledgebase

How to create project using High-performance Embedded Workshop V.4?

Latest Updated:12/09/2009


[High-performance Embedded Workshop V.4] I want to create a new project for another product, based on the project which already has finished developing. Are there any good tips for this?
I tried to copy the workspace folder, but it was not perfect because the project name was succeeded.


The function of Custom project types is available. This allows you to select the same project as file structure, build option and so from project type when creating new project. Also Custom project types allow you to export to another user environment.
Refer to the following for the detail of Custom project types.

  • High-performance Embedded Workshop V.4.xx user's manual
    Custom project type

You can download the user's manual from document page.

Suitable Products
High-performance Embedded Workshop