Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

How to use the HEW on the WindowsNT family's OS?

Latest Updated:09/10/2007

Question:

[High-performance Embedded Workshop V.4, V.3]  How can I use the high-performance Embedded Workshop on the WindowsNT family's OS.

Answer:

[In case of using High-performance Embedded Workshop4]

1, Install the high-performance Embedded Workshop on PC by administration authority.

2, Keep the folders used through High-performance Embedded Workshop accessibe.

[In case of using High-performance Embedded Workshop3]

1.Install

Install as an administrator.

2.Changing the environment variable

Do the following setup after closing workspace.

Select [Administration] from [Tools] on the High-performance Embedded Workshop menu

Open a Toolchain folder on [Registered components], and click toolchain displayed and click a [Properties] button.

Select CH38(for H8) and SHC_TMP(for SH) on a [Environment] tab, and click a [Modify] button. Move [Value] into the folder which has an access authority.

EG:Temporary directory - $(TEMPDIR)

Suitable Products
High-performance Embedded Workshop