Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Is the no. of cycles reflected to external memory's number of states?

Latest Updated:09/10/2007

Question:

Is the number of cycles which are displayed by performance analysis reflected to the external memory's number of states which is set into the control register?

Answer:

No. It does not reflect the control register settings. The number of cycles is calculated depending on the number of states set by the memory map.
Suitable Products
High-performance Embedded Workshop
Simulator Debugger for SuperH Family [for High-performance Embedded Workshop]
Simulator Debugger for H8SX, H8S, and H8 Families [for High-performance Embedded Workshop]