Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Why if I debug the C source program info cannot be displayed?

Latest Updated:09/10/2007

Question:

I want to debug the C source program, but the debug information cannot be displayed. Why?

Answer:

In case of building by HEW, all of the following conditions must be satisfied in order to debug the program at a source level.

  • The debug options are being selected to both the compiler and the optimizing linkage editor

  • The code=machinecode option is being selected to the compiler as an output file type
    (If you select code=asmcode option, debagging at a source level is not available)

  • The form=absolute option is being selected to the optimizing linkage editor

  • The load module has been loaded to the Simulator or Emulator

 

 

Please see the file below also

 

 

Please see the file below

 

Suitable Products
High-performance Embedded Workshop