Skip to main content
Renesas India - Knowledgebase

Does warning requires processing in response?

Latest Updated:11/21/2014


Reading by CubeSuite+ of the project file (r_fsl_praxis01.mtpj) in the sample program described in the RL78/G13 Flash Self Programming: Execution application note leads to warnings W0071 and W0072. Does this require any processing in response?


Warnings W0071 and W0072 are generated when the relink function for the boot and flash areas is used by the project file for the sample program, and no processing is needed.
Suitable Products
Flash Self Programming Libraries