Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

How to change the version of the compiler with a CS+ project?

Last Updated:06/14/2017

Question:

How do I change the version number of the compiler for use with a CS+ project?

Answer:

Select the [Common Options] tabbed page on the [Property] panel for the build tool. Select [Using compiler package version] under the [Version Select] category.
Since the setting [Always latest version which was installed] is selected by default, the version number of the compiler for use with projects is automatically changed when the version of CS+ or the compiler is updated.

You can change or fix the version of the compiler to be used by specifying a version number as described above.

For details, see this Online Help.

Suitable Products
CS+ (formerly CubeSuite+)