Skip to main content
Renesas India - Knowledgebase

Perform step in execution of CubeSuite+ when debugging user program?

Latest Updated:04/04/2014


Is it possible to perform step-in execution of CubeSuite+ when debugging a user program which incorporates the libraries for the RL78 family of MCUs listed below?

  • Flash Self Programming Library Pack01
  • Data Flash Library Type04
  • EEPROM Emulation Library Pack01
  • EEPROM Emulation Library Pack02


Debugging procedures such as step-in execution will work with the user program, but might not proceed normally within the functions of the various libraries. Therefore, only use debugging by step-in execution on the user program.
Suitable Products
Flash Self Programming Libraries
Data Flash Libraries