Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Q0140035 Message_CS+

Last Updated:12/20/2017

Question:

When I tried to use the integrated uninstaller of the CS+ integrated development environment, the Q0140035 message appeared. What should I do about the message?

Answer:

When the rapid start function of CS+ is enabled, CS+ stays resident for improved startup speed. Right-click on the CS+ icon in the notification area (system tray) and select [Exit] to terminate CS+. Then, use the integrated uninstaller.
 

Suitable Products
CS+ (formerly CubeSuite+)
  • Was this article helpful?