Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Reference of Description of SFR and IOR_CS+

Last Updated:10/11/2017

Question:

I am using the CS+ for CC integrated development environment. Can I refer to the description of SFR and IOR of an MCU while editing?

Answer:

Use the Smart Manual for the CS+ for CC integrated development environment.

You can quickly view the description of SFR (Special Function Register) or IOR (I/O Register) in the following panels by simply moving the mouse cursor over the register. (RL78 and RX only)

Editor panel
SFR/IOR panel
Disassemble panel
Watch panel
This function is available in CS+ for CC V6.00.00 and later.
See here for details about the Smart Manual.
 

Suitable Products
CS+ (formerly CubeSuite+)
  • Was this article helpful?