Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Saving of Tools and Settings for Development_CS+

Last Updated:12/20/2017

Question:

I am using the CS+ integrated development environment. I would like to back up the build settings and tools for development to restore them later. What should I save?

Answer:

Use the “Save Project and Development Tools as Package” function in the CS+. You can save a set of a project and tools together by this function.
For details about this function, see here.
 

Suitable Products
CS+ (formerly CubeSuite+)
  • Was this article helpful?