Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Why description of the default settings only contains in wsetup.c?

Latest Updated:02/26/2015

Question:

It seems that the start menus have been divided into two types from CS+ V3.00.00. What differences are there?

Answer:

Selection of the start menu depends on the compiler you are using.

CC-RX compiler (RX family) CS+ for CC (RX, RH850)
CC-RH compiler (RH850 family) CS+ for CC (RX, RH850)
CA78K0R compiler (78K family: 78K0R) CS+ for CA, CX (78K, RL78, V850)
CA78K0R compiler (RL78 family) CS+ for CA, CX (78K, RL78, V850)
CA78K0 compiler (78K family: 78K0) CS+ for CA, CX (78K, RL78, V850)
CA850 compiler (V850 family: V850E) CS+ for CA, CX (78K, RL78, V850)
CX compiler (V850 family: V850E2) CS+ for CA, CX (78K, RL78, V850)

If you double-click on the project file, CS+ for that project type will be started.

Suitable Products
CS+ (formerly CubeSuite+)