Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

A View window has gone. How can I restore it?

Latest Updated:12/11/2014

Question:

A View window has gone. How can I restore it?

Answer:

A View window can be activated by selecting "Window"->"Show View" menu.
Selecting "Window"->"Reset Perspective" menu would restore all View layouts.
"Reset Perspective" restores current active perspective View layouts, as well as all menus and buttons back to the default layout.
That is, restoring the default layout of view , menus, and buttons on current  perspective (C/C++ or debug.)
Suitable Products
e² studio