Skip to main content
Renesas India - Knowledgebase

Commandline build of e² studio project

Last Updated:09/06/2017


How do I build an e² studio project as a Windows command not via GUI?


In the e² studio installation folder, you will find the commandline version eclipse named "eclipsec.exe" with standard GUI based e2studio.exe.
Build operations can be performed as a command with the eclipsec.exe.
For more details about this issue, see the e2 studio Help at "Using e² studio in Hudson/Jenkins".
Suitable Products
e² studio
RZ Family