Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

How to suppress "Type '***' could not be resolved" code analysis error?

Latest Updated:01/22/2016

Question:

How to suppress "Type '***' could not be resolved" code analysis error?

Answer:

This warning is generated by CODAN (Code Analysis function); a part of the eclipse standard C development plugin CDT.
Solutions are described for each cases.

[Case1: Warned for compiler's internal symbol or keyword]
This issue may be caused by compiler specific symbols (so called "keyword", e.g. __far) because CODAN can't recognize symbols which are not defined on any header files.

In such cases, adding any of the following declarations would solve this issue. Please consult the compiler manuals for the specific symbols.

code example for RX Family C/C++ Compiler Package (CC-RX)

#ifdef __CDT_PARSER__
#define near
#define _near
#define far
#define _far
#define __evenaccess
#endif

code example for RL78 Family C Compiler Package (CC-RL)

#ifdef __CDT_PARSER__
#define __near
#define __far
#define __saddr
#endif

[Case2: Symbols are undefined, or lacking for header file path settings]
CODAN tries to solve symbols in header files based on "include path" setting.
The error in this title occurs if symbols were not found.
Please visit "C/C++ General" -> "Paths and Symbols" of project property and check "include
directories" file paths.

Suitable Products
e² studio