Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Why e2 studio Help tree's [+][-] buttons are not working?

Latest Updated:12/03/2014

Question:

e2 studio Help tree's [+][-] buttons are not working and only contents top pages can be seen.

Answer:

[Possible cause]
Internet Explorer is used as e2 studio Help viewer. Some version of Internet Explorer may not show pages as expected because of compatibility issues.

[Workaround]
Internet Explorer's compatible mode can solve this kind of compatibility issues.
To do so, add the following line after "-vmargs" in the e2studio.ini file located in e2 studio installed folder.

-Dorg.eclipse.swt.browser.IEVersion=7000

Note: Terminate e2 studio before editing the ini file.
Suitable Products
e² studio