Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Off-board Writing to Flash Memory

Last Updated:02/05/2018

Question:

How do I write off-board to the flash memory of the RL78/G1D or RL78/G1D module (RY7011)?

Answer:

Create a conversion board jig, such as a socket adapter, and write according to the description in user's manual for the RL78/G1D or RL78/G1D module (RY7011).

・RL78/G1D User's Manual: Hardware (R01UH0515)
  "26.1 Serial Programming Using Flash Memory Programmer"
https://www.renesas.com/search/keyword-search.html#q=R01UH0515&genre=document
  
・RL78/G1D Module (RY7011) User’s Manual: Hardware (R02UH0004)
  " 3.1 Serial Programming Using Flash Memory Programmer"
https://www.renesas.com/search/keyword-search.html#q=R02UH0004&genre=document

Suitable Products
RL78/G1D
Bluetooth
  • Was this article helpful?