Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Transmit iBeacon data using the RL78/G1D module (RY7011)

Last Updated:09/20/2017

Question:

Is it possible to make the RL78/G1D module (RY7011) supported to iBeacon via API control from the host microcomputer?

Answer:

It is possible to supported by setting iBeacon format data to the adv_data parameter of RBLE_GAP_Broadcast_Enable function.
iBeacon format specifications can be downloaded from "Download Artwork and Specifications" at the bottom right of the page of the following URL. (* Consent to iBeacon license agreement is required.) 
https://developer.apple.com/ibeacon/
Suitable Products
RL78/G1D
Bluetooth