Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Adaptable Function Introduction

Last Updated:02/13/2017

Question:

What is the purpose of the Adaptable Function?

Answer:

When enabled, the Adaptable Function automatically selects the optimum balance between power consumption and communication range. This feature available in RL78/G1D MCUs is for use only in slave devices.

By default, the Adaptable Function is turned off. Set it to ON when desired.

The Adaptable Function switches between three modes according to the master device's signal strength as perceived by the slave device according to the list below.

• Low power mode to normal mode, normal mode to low power mode → near -50 dBm
• Normal mode to high performance mode, high performance mode to normal mode → near -70 dBm

Suitable Products
RL78/G1D
Bluetooth