Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

What is "IT800"?

Latest Updated:09/15/2006

Question:

What is "IT800"?

Answer:

One of PLC core which Itran developed. Low speed (7.5 kbps to 1.25 kbps at 100 kHz to 400 kHz)
Suitable Products
M16C/6S
EV5-ASIA (R0K3306S0D011BR)
EV5-US (R0K3306S0D010BR)
SDK-PLC-EU-A (or -B for CENELEC B band)
  • Was this article helpful?