Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

How will I know if an EPROM or microcontroller is made from Japan?

Latest Updated:05/01/2007

Question:

How should I judge whether an EPROM or a flash memory microcontroller is in compliance with the Japanese Trade Control Act?

Answer:

For rewritable flash memory microcontrollers, the microcontroller main unit (hardware) is judged as a general-purpose integrated circuit. A program written to a flash memory must be judged separately from the microcontroller main unit (hardware).
The same applies to the EPROM microcontrollers. If an EPROM microcontroller can be rewritten, the microcontroller main unit (hardware) is judged as a general-purpose integrated circuit, and a written program must be judged separately from the microcontroller main unit (hardware).
Please consult a Japanese sales representative or distributor for further questions.
Suitable Products