Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Does the sample program run on a standalone PC ?

Latest Updated:12/01/2011

Question:

Does the sample program run on a standalone PC ?

Answer:

No, it cannot be executed as is.
If a simulator is also running on the PC, the program runs as well.
Otherwise, it cannot be operated on a standalone PC.
Suitable Products