Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

What is the reason why the system enters the wait status?

Latest Updated:12/01/2011

Question:

Even if there is enough space available, when get_blk is executed, the system enters the wait status.
Is there any way of analyzing the cause of this?

Answer:

Use the task debugger (RD850 Pro) in a case like this.
You can check the wait status of the memory pool using the RD850 Pro.
Suitable Products
  • Was this article helpful?