Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Is it OK if the interval during reset signal is input lasts for a while?

Latest Updated:12/01/2011

Question:

Is it OK if the interval during which the reset signal is input lasts several seconds?

Answer:

Yes, there is no problem to input the reset signal for a long time.
While there is a restriction as to how short the reset signal can be, there is no such restriction about how long it can be.
Suitable Products
RL78 Family
78K Family